Mi carpeta/Enviar SolicitudAyuda
TURCK alrededor del mundo
Mapa del Sitio

por palabra clave  |  Tips  
Número telefónico:
 
tiempo de:
Horario de Verano
TURCK Connect


03 de Octubre de 2007

Productos de Sensores

detallesLanzamiento de Prensa          detallesAlta resolución          productoProducto


Stainless Steel Front Face Sensors from TURCK

 

Minneapolis, Minn. - TURCK has added new stainless steel front face sensors to its line of harsh duty sensors. These durable sensors are designed to withstand the physical abuse often found in the automotive industry.

These sensors use one-piece stainless steel construction for the barrel and sensing face, delivering an IP 68 and 69k protection rating against moisture and fl uid ingress. This also prevents corrosion and allows the sensor to be used in areas where oil, lubricants and chemical washdowns occur, like those found in food and beverage applications.

The sensors are available in 12, 18 and 30 mm barrels, with a 3-wire DC quick disconnection. The sensor is an ideal replacement for sensors that use other face material, like plastic, that cannot withstand physical abuse.


 
Imprimir esta páginaImprimir esta página    |     |ComentariosContáctenos / E-mail lista     | Inicio de la páginaInicio de la página