Mi carpeta/Enviar SolicitudAyuda
TURCK alrededor del mundo
Mapa del Sitio

por palabra clave  |  Tips  
Número telefónico:
 
tiempo de:
Horario de Verano
TURCK Connect


28 de Diciembre de 2007

Productos de Sensores

detallesLanzamiento de Prensa          detallesAlta resolución          productoProducto


Un sensor de presión que coloca el control en las manos del Usuario

 

Minneapolis, Minn. - TURCK introduces a new programmable output high accuracy pressure sensor that allows the user to select the output as either two switch points or a 4-20 mA analog output with one switch point. The switch points are PNP/NPN programmable, and provide fl exibility for applications where the output requirements are unclear.

“Furthermore, TURCK sensors with ranges from 1 to 40 bar had their ranges extended to -1 bar,” notes Melissa Henning, product specialist with TURCK’s sensor division. “This allows the switch point or analog start point to be programmed in the vacuum range to detect pressure in a positive pressure unit if the application requires it.”

In addition to the programmable output, these sensors also allow the user to select units of pounds per square inch, bar, inches of water, feet of water, millibar, inches of Mercury, meters of water, and kilograms per square centimeter. The user can simply choose the display most relevant to the application.

The sensor’s stainless steel construction provides an IP 67 protection rating, and rotating and non-rotating housings are available. A UV resistant cover for use in outdoor applications is also available with the sensor.


 
Imprimir esta páginaImprimir esta página    |     |ComentariosContáctenos / E-mail lista     | Inicio de la páginaInicio de la página