Mi carpeta/Enviar SolicitudAyuda
TURCK alrededor del mundo
Mapa del Sitio

por palabra clave  |  Tips  
Número telefónico:
 
tiempo de:
Horario de Verano
TURCK Connect


May 8, 2007

Productos de Sensores

detallesLanzamiento de Prensa           detallesAlta resolución          productoProducto


Magnetic Flow Meters from TURCK

 

Minneapolis, Minn. - TURCK Inc introduces new FCMI flow meters that measure flow rates between 0 and 9.9 gallons per minute. FCMI meters use the magnetic inductive principle to detect flow in a range of electrically conductive fluids.

FCMI flow meters have an accuracy rating of 2 percent of the measured value. Unlike paddle wheel or vortex fl ow meters, FCMI flow meters do not obstruct the flow of the media to obtain a measurement. In fact, FCMI flow meters have no moving parts to experience wear and tear, virtually eliminating early replacements. The flow meters may be applied in many industries including water treatment, steel, machine engineering, chemical, pharmaceutical and energy.


 
Imprimir esta páginaImprimir esta página    |     |ComentariosContáctenos / E-mail lista     | Inicio de la páginaInicio de la página